Search FAQs
What is the part number of a potentiometer that can be used on Schneider drive?
Issue:
Is there a Potentiometer available for an AC drive?
Product Line:
All Altivar Drives
Environment:
All
Cause:
Customer needs a speed pot for an Altivar drive.
Resolution:
Most of the drives will accept any potentiometer rated between 1k Ohms and 10 k Ohms, 1/2 Watt. See the installation user guide for the specific drive that you are using to determine the specific range that it can use.
Part number ATVPOT25K is a complete 22mm operator with mounting collar and 2.5K ohm potentiometer that has been a standard part number for many years (drawing attached for reference). However, this part is in the process of being phased out.
The E-Flex, M-Flex and MCC `s all use the ZB5AD922 operator in conjunction with part # 80442-273-02 (2.5k ohm pot)
Suggest using one of the following:
For 22mm
Metal - XB4BD912R10K
Plastic - XB5AD912R10K
For 30mm
Metal - 9001K2108
Plastic - 9001SK2108
Is there a Potentiometer available for an AC drive?
Product Line:
All Altivar Drives
Environment:
All
Cause:
Customer needs a speed pot for an Altivar drive.
Resolution:
Most of the drives will accept any potentiometer rated between 1k Ohms and 10 k Ohms, 1/2 Watt. See the installation user guide for the specific drive that you are using to determine the specific range that it can use.
Part number ATVPOT25K is a complete 22mm operator with mounting collar and 2.5K ohm potentiometer that has been a standard part number for many years (drawing attached for reference). However, this part is in the process of being phased out.
The E-Flex, M-Flex and MCC `s all use the ZB5AD922 operator in conjunction with part # 80442-273-02 (2.5k ohm pot)
Suggest using one of the following:
For 22mm
Metal - XB4BD912R10K
Plastic - XB5AD912R10K
For 30mm
Metal - 9001K2108
Plastic - 9001SK2108
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: