{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How long can the motor leads be on a ATV212 S-flex Drive?

Issue:
Motor leads length on a ATV212 S-flex

Product Line:
ATV212

Environment:
Motor Wiring

Cause:
n/a

Resolution:
The longer the cable, the greater the capacitance. Cable lengths greater than 164 ft (50 m) may appear as a ground fault condition to the drive.  For installations where cable capacitances may be a problem, a reactor or motor protection filter can be installed between the drive and the motor.

The S-Flex is not intended to be used where extremely long output cable runs are required.  Maximum output cable length for standard duty motors should be limited to 100 m (328 ft).  For applications exceeding this cable length, consult the Drives Application Engineer.


Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: