{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the length of the power cords of an ACSC

Issue:
What are the length of the power cords of an ACSC.

Product line:
ACSC100, ACSC103.

Environment:
All Product models, all serial numbers.

Cause:

Resolution:

ACSC Power cord lengths

60 Hz unit – 5.5 Feet (1.7 m)

50 Hz unit – 12 Feet (3.6 m)

Schneider Electric Saudi Arabia

Attachment(s)
K-B ACSC Power cord lengths.doc [23.5 KB]