{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What control voltage is needed for an ATS01N1..FT softstart?

Article available in these languages: Spanish

Issue:
Does the ATS01N1..FT need control voltage for running?


Product Line:
Altistart 01


Environment:
All


Cause:
N/A


Resolution:
The ATS01..FT models accommodate several control voltage options:
110 - 230Vac can be connected to terminal CL2 and neutral to CL1/0
24Vac or 24Vdc can be connected (+) to terminal 24V and (-) to CL1/0

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: