{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
When do the ATS48 internal cooling fans run?
Issue:
ATS48 Fan Specification

Product Line:
Altistart 48

Environment:
All

Cause:
NA

Resolution:
ATS48D17Y and ATS48D22Y do not have fans.  All other models do have fans.
The fans will operate when the heatsink temperature is greater than 50C.
The fans will stop operating when the heatsink temperature drops below 40C.


Schneider Electric Saudi Arabia