{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can the ATV212 or ATV21 be set up for start/stop on terminal and ramp to 60 Hz?

Issue:
ATV212 or ATV21 set up to start/stop on terminal and ramp to 60 Hz

Product Line:
ATV21, ATV212

Environment:
All models and serial numbers.

Cause:
None

Resolution:
Begin by wiring the remote start switch or relay for two wire control between terminals P24 and F.

Program the nameplate motor parameters into the following parameters:

CODE - DESCRIPTION
thr - Motor thermal prot.
uLu - Motor rated voltage
F415 - Motor rated current
F417 - Motor rated speed


Make the following parameter settings:

CODE - DESCRIPTIONSETTING
LL - Low limit frequencyas desired
UL - Upper limit freq60
Dec - Deceleration ramp timeas desired
ACC - Acceleration ramp timeas desired
CMOD - Command mode selection0

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Schneider Electric Saudi Arabia