Search FAQs
Video: What is minimum firmware version required for the ATV71 or ATV61 to use the VW3A3316 Ethernet IP card?
Issue:
What is minimum firmware version required for the ATV71 or ATV61 to use the VW3A3316 Ethernet IP card?
Product Line:
VW3A3316
Cause:
ATV71 & ATV61 have minimum firmware required to use the VW3A3316 Ethernet IP card
Resolution:
This communication option card is fully supported with the version V1.5 IE 13 and above of the Altivar 61 firmware. This communication option card is only supported with the version V1.6 IE 19 and above of the Altivar 71 firmware. Specific versions of the Altivar 71 firmware are not supported.
What is minimum firmware version required for the ATV71 or ATV61 to use the VW3A3316 Ethernet IP card?
Product Line:
VW3A3316
Cause:
ATV71 & ATV61 have minimum firmware required to use the VW3A3316 Ethernet IP card
Resolution:
This communication option card is fully supported with the version V1.5 IE 13 and above of the Altivar 61 firmware. This communication option card is only supported with the version V1.6 IE 19 and above of the Altivar 71 firmware. Specific versions of the Altivar 71 firmware are not supported.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Category:
Explore more
Range:
Category: