{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the default control board for the ATV212 (or ATV21) drive be purchased as an individual part?
Issue:
Control board for the ATV212 (or ATV21) drive replacement

Product Line:
Altivar ATV21 and ATV212

Environment:
All

Cause:
Needs to replaced the basic control IO card that was in the ATV21 or ATV212 drive.

Resolution:
No. This part is not available to purchase in the US.

Schneider Electric Saudi Arabia