{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I change the motor direction if the motor is rotating right in drive mode but not in bypass mode?
Issue:
How can I change the motor direction in drive mode and bypass mode?

Product Line:
All enclosed with a bypass option

Environment:
All

Cause:
Motor is running in the correct direction in drive mode and reverse in bypass mode.

Resolution:
-If the motor runs the correct direction from the drive but the wrong direction in bypass, swap any 2 incoming power leads into the cabinet.
-If the motor runs the correct direction in bypass but the wrong direction from the drive, swap any 2 motor leads coming out of the drive on UVW
or you can change the programming phase rotation in menu 1.1 simple start menu from ABC to ACB.

Schneider Electric Saudi Arabia