{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What indicates that the internal bypass contactor has closed on the ATS22 soft starter?
Issue:
Needs ATS22 indication that the internal bypass contactor is closed

Product line:
Altistart 22

Environment:
All models, all serial numbers

Cause:
The bypass contactor is internal and cannot visually be seen

Resolution:
For remote indication, assign one of the relays to the "run" function.  The relay is energized when the bypass contactor is closed.  The relay dry contact can be used in a control circuit for the remote indication.

For local indication, check the RUN indicator LED just above the integral display.  The yellow LED will be continuously ON when the internal bypass contactor is closed.

Schneider Electric Saudi Arabia