{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the filter material in the side vent hoods of a NEMA 3R E-Flex drive?
Issue:
Part number for the filter material in the side vent hoods of a NEMA 3R E-Flex drive

Product Line:
E-Flex

Environment:
Nema 3R enclosures

Cause:
Require replacement filters

Resolution:
Per E-Flex manual, the 3R filter material is 31158-441-01.  Qty = 2 per E-Flex.

Since the E-Flex product line is obsolete, the manufacturing plant no longer procures this item.
Recommendation:
Standard foam filter material of 10 ppi (pores per inch) can be used.
This is available from a number of sources and can be cut to size.

Dimensional drawings are attached.

Schneider Electric Saudi Arabia

Attachment(s)
80444-205-01.pdf [57.09 KB]
31158-441-01.pdf [38.02 KB]