Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Where can I download SoMove and DTM files?

Article available in these languages: Czech, Spanish, Norwegian


Issue:
Where can I find a link for SoMove?

Product line:
Variable Frequency Drives and Soft Starts  

Environment:
All models, all serial numbers   

Cause:  
None

Resolution: 
Below are the Links for SoMove Software and DTMs for AC Drives and Softstarts. 

(SoMove: latest version)
https://www.se.com/us/en/download/document/SoMove_FDT/

(Altivar DTM files for the ATV61, ATV71, ATV12, ATV212, ATV312, ATV32)
(Altivar Process 600 DTM files)
https://www.se.com/us/en/download/document/ATV6xx_DTM_Library_EN/

(Altivar Process 900 DTM files)
https://www.se.com/us/en/download/document/ATV9xx_DTM_Library_EN/

(Altistart DTM files for ATS22 and ATS48)
https://www.se.com/us/en/download/document/Altistart_DTM_Library/

All other:
https://www.se.com/us/en/download/doc-group-type/3587139-Software & Firmware/?sortByField=Popularity
 
Click on Optional Filters
Select Document Type Group: Software/Firmware
Select a Product Category - Variable Speed Drives and Softstarts
Select a Product Sub-Category - Low Voltage AC Process Drives
Select Product Range -
-  Altivar 61 (i.e. for all Altivar AC Drives DTM)
-  Altistart 48 (i.e. for Altistart Softstarts DTM)
-  Process
-  etc.
Click the Search button
 
Download the DTM files for Altivar drives and the stand alone file for Somove.
 
WinZip or 7-Zip Extraction software may be needed for compressed/zipped files.  If needed you can Download Free version 7-Zip from;  http://www.7-zip.org/
 
The  USB to RJ45 cable part number is TCSMCNAM3M002P
The SoMove software is free online, however, you will need to purchase this cable to connect your PC to products via the resident Modbus port.
The USB cable is not required if the Drive has an available Ethernet communication port available. 
The drivers for the USB cable are included as part of the SoMove software.
When installing SoMove, make sure the USB cable is not connected.  Only after the installation completes should you connect the cable to  the PC.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: