{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the power consumption of the fans in the NetShelter CX?

Issue:
There's a needs to know how much power is consumed by the NetShelter CX fans.

Product Line:
NetShelter CX

Environment:

All versions and serial ranges.

Cause:
It may be important to calculate total power consumption

Resolution:

NetShelter CX Mini = 30W
NetShelter CX/CX2 18U = 34W
NetShelter CX/CX2 24U = 68W
NetShelter CX/CX2 38U = 101W

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: