{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Thermal Capacity of the NetShelter CX Mini and CX2?
Issue:
Define the thermal capacity of the NetShelter CX.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Know the thermal capacity so that it's not exceeded.

Resolution:
AR4000MV NetShelter CX Mini = 800W
AR4018A / AR4018IA NetShelter CX 18U = 1.2kW
AR4024A / AR4024IA NetShelter CX 24U = 2.4kW
AR4038A / AR4038IA NetShelter CX 38U = 3.6kW.
Calculate the internal load by adding together the power ratings of the installed equipment.

Schneider Electric Saudi Arabia