{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the NetShelter CX be deployed in any room or space?
Issue:
Where can the NetShelter CX be deployed?

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
It's wise make sure that the NetShelter CX is suited for the environment in which it's to be installed.

Resolution:
Optimal performance of these cabinets requires suitably ventilated space or building HVAC system.
The NetShelter CX is not suitable for installation in a small unventilated space.

Schneider Electric Saudi Arabia