{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I find a copy of the ATV61 Installation Manual?
Issue:
Installation manual needed for an Altivar 61 Drive

Product line:
Altivar 61

Environment:
All models, all serial numbers

Cause
Installation manual is not shipped with the drive.

Resolution:
There are two Installation manuals for the ATV61 drives, Low HP (up to 100HP) and High HP (above 100HP).

The installation manual for the Altivar 61 drives up to and including 100 Horsepower can be found at this link: https://www.se.com/us/en/download/document/1760643/
The installation manual for the Altivar 61 drives above 100 Horsepower can be found by following this link: https://www.se.com/us/en/download/document/1760655/

Schneider Electric Saudi Arabia