Issue:
Is Brake Logic Control Avilable in the ATV32 Drive?
Product line:
Altivar 32, ATV32
Environment:
All models, all serial numbers
Cause:
NA
Resolution:
ATV32 drive does have Brake Logic Control function parameters.
Refer to the ATV32 Programming manual, ATV32_programming_manual_S1A28692_01
Is Brake Logic Control Avilable in the ATV32 Drive?
Product line:
Altivar 32, ATV32
Environment:
All models, all serial numbers
Cause:
NA
Resolution:
ATV32 drive does have Brake Logic Control function parameters.
Refer to the ATV32 Programming manual, ATV32_programming_manual_S1A28692_01
Released for:Schneider Electric Saudi Arabia