{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is a USF fault on the ATS48 (or ATS46) Soft Starters?
Issue:
Why is my ATS48 tripping on USF faults?
Product line:
Altistart ATS48 and ATS46
Environment:
All models, all serial numbers
Cause:
When a Run command is given, the mains voltage on L1 L2 L3 is absent for 350msec.
Resolution:
The soft start checks for three-phase AC power at the L1, L2, and L3 terminals as soon as a RUN command is received. This fault appears if the soft start has a RUN command and does not have line power in all three phases within 350 ms. This fault is stored in the fault history. Probable cause on a soft start with separately supplied control power:
• The line-supply circuit breaker, line fuses, or isolation contactor is open.
• The power board is defective.
• Determine why the three-phase power is not present at the L1, L2, and L3 terminals of the soft start when it receives a RUN command. Rectify the power supply problem.
• Verify the soft start's line voltage detection circuit by supplying only control voltage and verifying that nLP displays. Then apply a three phase line voltage and verify that RDY displays. If not, verify all internal soft start connections. If no problem is found, replace the power board.

Schneider Electric Saudi Arabia

Attachment(s)
ATS48 Y Range basic.pdf [1.78 MB]