{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a VW3A1101 keypad be used on the ATV312 to transfer programs?
Issue:
Store and transfer program files using VW3A1101 keypad.

Product Line:
Altivar ATV312

Environment:
All models, all serial numbers.

Cause:
A duplicate program is to be used on multiple drives.

Resolution:
No.  Although the VW3A1101 is compatible with ATV312, it cannot be used to transfer a program file from one ATV312 to another.  A Multi-Loader or Simple Loader tool or SoMove software can be used to transfer files.

Schneider Electric Saudi Arabia