Search FAQs
What is the cause of the EF2 fault code on the ATV21 and ATV212 drives?
Issue:
ATV212: EF2 Fault
Product line:
Altivar ATV212
Environment:
All models, all serial numbers
Cause:
Ground Fault on the output of the drive.
Resolution:
EF2= Ground Fault
Troubleshooting tips
Reference the ATV212 programming manual S1A53838 (attached).
ATV212: EF2 Fault
Product line:
Altivar ATV212
Environment:
All models, all serial numbers
Cause:
Ground Fault on the output of the drive.
Resolution:
EF2= Ground Fault
Troubleshooting tips
- Check the motor ground connections. Make sure the ground is going to the chassis of the drive.
- Remove the motor leads from the drive and Megger with a 1KV Megger to see if there is a short to ground in the motor windings.
Reference the ATV212 programming manual S1A53838 (attached).
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: