{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: INF6 error on the ATV61 and ATV71 drives

Issue:
What is INF6 Fault on Altivar 61 & 71 Drives?

Product Line:
Altivar ATV61 and ATV71

Environment:
All products

Cause:
The control terminal card may be loose or there may be 2 serial communication cards installed at once.

Resolution:
INF6 is an internal option fault.  Basically, the option card installed on the VFD is not recognized.
First, re-seat the control terminal card.  Then, check the 1.11 Identification menu for option 1 and option 2 to see if there are 2 conflicting option cards installed.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: