{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Will the relay output, assigned to No Drive Fault, change states on a fault if Auto restart is set to yes on VFD?

Issue:
State change on relay assigned to No Drive Fault

Product Line:
Altivar 61 Altivar 71 ATV61  ATV71

Environment:
All

Cause:
Define the No Drive Fault relay relationship with Auto restart function.

Resolution:
The relay assigned to No Drive Fault will not change states on a fault if Auto restart (Atr) is set to YES until the max restart time (tAr) is depleted and the fault still exists.

Schneider Electric Saudi Arabia

Explore more
Range:
Altivar 71Altivar 61
Explore more
Range:
Altivar 71Altivar 61
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.