Issue:
is EMC Filter built-in on ATV61?
Product Line:
Altivar 61
Environment:
All models except the ATV61H...M3X series.
Cause:
None
Resolution:
Altivar 61 drives, except for the ATV61H...M3X, have built-in radio interference
input filters to meet the EMC standard for variable speed electrical power drive
“products” IEC/EN 61800-3, edition 2, category C2 or C3 in environment 1 or 2 and
to comply with the European directive on EMC (electromagnetic compatibility).
is EMC Filter built-in on ATV61?
Product Line:
Altivar 61
Environment:
All models except the ATV61H...M3X series.
Cause:
None
Resolution:
Altivar 61 drives, except for the ATV61H...M3X, have built-in radio interference
input filters to meet the EMC standard for variable speed electrical power drive
“products” IEC/EN 61800-3, edition 2, category C2 or C3 in environment 1 or 2 and
to comply with the European directive on EMC (electromagnetic compatibility).
Released for:Schneider Electric Saudi Arabia