{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Need assistance selecting the parts required for single phase input to a VFD to run a 3 phase motor.

Issue:
Needs to run a 3 phase motor with 1 phase input voltage.

Product Line:
ATV61
ATV71
ATV312
ATV320
ATV12
ATV630
ATV32
ATV930

Environment:
All

Cause:
Customer only has single phase input power but needs to run a 3 phase motor.

Resolution:
Several of our drives have been tested and approved to accept single phase input power to run 3 phase motors.
Drives must be derated to handle the increased current on the input bridge and increased ripple or noise on the DC Bus.
In some cases input line reactors may be required or may allow higher SSCR ratings.

Consult the appropriate Quick Start Guide Annex.  These documents also provide fuse and circuit breaker information.

ATV630
Only recommended on single phase for pump application (Altivar Process Drive) : https://www.se.com/ww/en/download/document/EAV64300/

ATV930
Not currently approved for use on single phase applications.

ATV320
(Constant or Variable Torque applications): https://www.se.com/ww/en/download/document/NVE21777/

ATV340
Not currently approved for use on single phase input applications

ATV12
(Constant or Variable Torque applications): https://www.se.com/ww/en/download/document/S1A58684/

The ATV212 is not capable of supporting single phase input applications.

For any other application requirements consult following 3rd party website (Bonitron).
http://www.bonitron.com/drive-schneider.html#regen3
The ATV930 product is recommended for use with this option.
Contact Bonitron directly for assistance.


OLDER product info:
ATV61
NOTE- product has been discontinued (Variable Torque applications):https://www.se.com/us/en/download/document/S1B86981/

ATV71
NOTE - product has been discontinued (Constant Torque applications):https://www.se.com/ww/en/download/document/S1B86988/

ATV312
NOTE - product has been discontinued (Constant or Variable Troque applications):https://www.se.com/us/en/download/document/S1B16328/

ATV32
NOTE - product has been discontinued (Constant or Variable Troque applications) :https://www.se.com/ww/en/download/document/S1B39941?showAsIframe=true





Schneider Electric Saudi Arabia