{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the appropriate replacement for an ATV11 drive?
Issue:
Needs a replacement part number for an ATV11 drive.

Product Line:
Altivar 11

Environment:
All models and serial numbers

Cause:
Determine the replacement for an ATV11 drive.

Resolution:
The recommended replacement for the ATV11 is the ATV12.  Select the ATV12 based on the motor horsepower, rated motor voltage and supply voltage (single or three phase).

Schneider Electric Saudi Arabia