{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the NetShelter shock pallet be reused?
Issue:
Some shock pallets are reusable, some are not.
Product Line:
NetShelter SX
Environment:
All models and serial ranges
Cause:
An integrator may want to use the shock pallet to make multiple shipments.
Resolution :
The NetShelter shock pallet is designed for a single use only. Please do not reuse the shock pallet after the first shipment with equipment installed.

Schneider Electric Saudi Arabia