Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Video: Is it possible to power the ATV61 or ATV71 drive with an external 24Vdc power supply?
Issue:
Powering up an ATV61 or ATV71 with an external 24Vdc control power supply only.

Product Line:
ATV61, ATV71

Environment:
All

Cause:
Drive initial programming and configuration.

Resolution: 
Yes, an external 24Vdc can be connected between P24 and 0V terminals to supply control voltage. This will allow you to power the control board and HMI to read drive information.
You cannot run a drive with this 24VDC.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: