{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the different media that can be used with the InRow ACRD units?
Issue:
What are the different media that can be used with the InRow ACRD units?

Product line:
ACRD100, ACRD101, ACRD200, ACRD201

Environment:
Data Center Cooling

Cause:

Resolution:
The InRow ACRD can be used with refrigerant R410A alone in an air-cooled system. In fluid-cooled systems, condenser water and water/glycol can be used in the piping loops.

Schneider Electric Saudi Arabia