{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are optional outdoor heat exchangers (OHE) available with the InRow ACRD?
Issue:
Are optional outdoor heat exchangers (OHE) available with the InRow ACRD?

Product line:
ACRD100, ACRD101, ACRD200, ACRD201

Environment:
Data Center Cooling

Cause:

Resolution:
APC has standard SKUs available for a limited set of outdoor condensers and fluid coolers. Additional OHEs may be configured and custom ordered with the help of Applications Engineering team. Standard lead times do not apply to these units.

Schneider Electric Saudi Arabia