Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
v6.1.2 Network Management Card 2 "Reset All" or "Reset to Defaults" Command Does Not Work

Article available in these languages: Russian


Issue

No matter where the requested action is issued from (Command Line or Web UI), the Reset All and Reset All - Exclude TCP/IP command does not work. This command is used to reset the Network Management Card to defaults, including or excluding your TCP/IP settings (IP address, subnet mask, and default gateway).


Web:
reset all page


Command Line Interface reference:


apc>resettodef ?
Usage: resetToDef -- Configuration Options
resetToDef -p <all | keepip>

Product Line

  • Network Management Card 2 (NMC2) - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/AP9635CH
Devices with an embedded Network Management Card 2 include (but are not limited to): Older model 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products.



Environment
  • All serial numbers
  • AOS firmware versions including:
    • v6.0.6
    • v6.1.1
    • v6.1.2
Cause

This issue is the result of a firmware bug present in the aforementioned firmware versions.


Resolution

This issue is addressed in AOS v6.1.3 and higher. In order to resolve the issue, you must have AOS v6.1.3 or higher but this may not be available for all applications. Each Network Management Card has an AOS and application file and they cannot be updated independently. Please check http://www.apc.com/tools/download/index.cfm to verify the latest versions available for your device. If no upgrade is available, some other options are outlined below.


1.) Choose Reset Only (available via the web UI) and select all or specific configuration items. Selecting all will not completely wipe the NMC though if that is required.


2.) Manually delete the required database to reset the settings. This can be done via Telnet, SSH, or FTP.

Telnet/SSH direct to the NMC:
  • Log in to the card with your username and password.
  • Type cd db
  • Type delete cfg2.db
  • Optional: To also remove the current TCP/IP settings, type delete net.db.
  • Type reboot in order to issue a required reboot to complete this action

FTP/SCP (Instructions provided are for Windows Command Prompt FTP client but you can use any client)
  • Log into the card with your username and password.
  • Type cd db
  • Type del cfg2.db
  • Optional: To also remove the current TCP/IP settings, type del net.db.
  • Type bye in order to disconnect the FTP session. The NMC will reboot immediately unless there is another active user session. When all active sessions are closed/terminated, the NMC will reboot.


3.) If you need to factory reset your device, another option is to format your device. This wipes flash memory and any remaining configurations entirely, including your current TCP/IP settings. This step can be done one of two ways:
  • Press and hold the NMC's pinhole reset button for 20+ seconds, ensuring the NMC's status LED is pulsing green during this time. When it changes to amber or orange, release the reset button to let the format function complete and for the NMC to complete its reboot process.
  • Issue the format command via the command line via telnet, SSH, or local console. Issue a reboot command to complete the process.




Schneider Electric Saudi Arabia

v6.1.2 Network Management Card 2 "Reset All" or "Reset to Defaults" Command Does Not Work

Issue

No matter where the requested action is issued from (Command Line or Web UI), the Reset All and Reset All - Exclude TCP/IP command does not work. This command is used to reset the Network Management Card to defaults, including or excluding your TCP/IP settings (IP address, subnet mask, and default gateway).


Web:
 
reset all page


Command Line Interface reference:


apc>resettodef ?
Usage: resetToDef -- Configuration Options
    resetToDef -p <all | keepip>
 
 

 
Product Line

 
  • Network Management Card 2 (NMC2) - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/AP9635CH
Devices with an embedded Network Management Card 2 include (but are not limited to): Older model 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products.

 

 

Environment
 
  • All serial numbers
  • AOS firmware versions including:
    • v6.0.6
    • v6.1.1
    • v6.1.2
       
Cause

This issue is the result of a firmware bug present in the aforementioned firmware versions.


Resolution

This issue is addressed in AOS v6.1.3 and higher. In order to resolve the issue, you must have AOS v6.1.3 or higher but this may not be available for all applications. Each Network Management Card has an AOS and application file and they cannot be updated independently. Please check http://www.apc.com/tools/download/index.cfm to verify the latest versions available for your device. If no upgrade is available, some other options are outlined below.


1.) Choose Reset Only (available via the web UI) and select all or specific configuration items. Selecting all will not completely wipe the NMC though if that is required.


2.) Manually delete the required database to reset the settings. This can be done via Telnet, SSH, or FTP.

Telnet/SSH direct to the NMC:
  • Log in to the card with your username and password.
  • Type cd db
  • Type delete cfg2.db
  • Optional: To also remove the current TCP/IP settings, type delete net.db.
  • Type reboot in order to issue a required reboot to complete this action

FTP/SCP (Instructions provided are for Windows Command Prompt FTP client but you can use any client)
  • Log into the card with your username and password.
  • Type cd db
  • Type del cfg2.db
  • Optional: To also remove the current TCP/IP settings, type del net.db.
  • Type bye in order to disconnect the FTP session. The NMC will reboot immediately unless there is another active user session. When all active sessions are closed/terminated, the NMC will reboot.


3.) If you need to factory reset your device, another option is to format your device. This wipes flash memory and any remaining configurations entirely, including your current TCP/IP settings. This step can be done one of two ways:
  • Press and hold the NMC's pinhole reset button for 20+ seconds, ensuring the NMC's status LED is pulsing green during this time. When it changes to amber or orange, release the reset button to let the format function complete and for the NMC to complete its reboot process.
  • Issue the format command via the command line via telnet, SSH, or local console. Issue a reboot command to complete the process.




 

Schneider Electric Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

I'd like to receive news and commercial info from Schneider Electric and its affiliates via electronic communication means such as email, and I agree to the collection of information on the opening and clicks on these emails (using invisible pixels in the images), to measure performance of Schneider Electric's communications and to improve them. For more details, please read our Privacy Policy.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.