{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What UPS models are officially supported by the AP9624 (UPS Interface Expander 2 SmartSlot Card)?



Issue

What UPS models are officially supported by the AP9624 (UPS Interface Expander 2 SmartSlot Card)?


Product Line

  • UPS Device Management
    • AP9624 - UPS Interface Expander 2 SmartSlot Card
  • Various APC UPS Models - single and three phase



Environment

  • AP9624
  • Supported UPS models listed below


Cause

The user is unsure if the AP9624 is supported in their device or AP9624 is not working properly and compatibility is not confirmed.


Resolution

The following UPS lines have been officially tested with the AP9624 UPS Interface Expander 2 SmartSlot Card by APC:

  1. Smart-UPS Model Types with the following prefix:
    1. SU
    2. SUA
    3. SURT
    4. SURTA
    5. SURTD
    6. SUM
    7. SMT
    8. SMX
    9. SRC
    10. SRT
    11. SUVT/Galaxy 3500

  1. All single phase Symmetra Model Types including:
    1. Symmetra (Power Array)
    2. Symmetra RM
    3. Symmetra LX



Note:
The AP9624 is intended to support the above UPS models which consist of both older and newer generation UPS types. All other SmartSlot enabled UPS models may work in conjunction with the AP9624, however, compatibility has not been verified by APC.

Note: Important configuration information for AP9624 in supported UPS models also available in knowledge base FA176957.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.