Search FAQs
Data Center Expert | Trial version VM appears to have 25 nodes available.
Issue:
Trial version of StruxureWare Data Center Expert appears to have 25 node license available.
Product Line:
StruxureWare Data Center Expert
Environment:
StruxureWare Virtual Appliance
AP94VMTRL (All Versions)
Cause:
The current default configuration of all StruxureWare Data Center Expert is that the system comes with a pre-installed 25 node license key. The Virtual Machine or VM version shows this same 25 node license key in the user interface however until activated, will only allow 5 nodes to be added to the system.
Resolution:
This is by design. It was done so APC did not need to add a 5 node key to just this one version. Once activated, the rest of the nodes can be used. To fully activate the DCE VM the VM Activation license (APVMACT) must be purchased and redeemed to the server.
Trial version of StruxureWare Data Center Expert appears to have 25 node license available.
Product Line:
StruxureWare Data Center Expert
Environment:
StruxureWare Virtual Appliance
AP94VMTRL (All Versions)
Cause:
The current default configuration of all StruxureWare Data Center Expert is that the system comes with a pre-installed 25 node license key. The Virtual Machine or VM version shows this same 25 node license key in the user interface however until activated, will only allow 5 nodes to be added to the system.
Resolution:
This is by design. It was done so APC did not need to add a 5 node key to just this one version. Once activated, the rest of the nodes can be used. To fully activate the DCE VM the VM Activation license (APVMACT) must be purchased and redeemed to the server.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: