{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
In Hyper-V, Virtual Machine shutdown is delayed when VM Migration is enabled.
Issue:
There is a delay proceeding with virtual machine shutdown when VM migration is enabled for Hyper-V.

Product Line:
PowerChute Network Shutdown v3.1 up to v4.3

Environment:
Windows Hyper-V

Cause:
If the VM Migration time is insufficient in attempting to migrate all VMs, there is a timeout issue before PowerChute proceeds with shutting down VMs that failed to migrate.

Resolution:
Ensure you allow sufficient time for the VM migration duration to attempt to migrate all VMs.

NOTE: This is is resolved in PoewrChute Network Shutdown v4.4. 
 

Schneider Electric Saudi Arabia

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.