We have two types of contactors the power contactors category (AC-1 for resistive loads ex: lighting ) and category AC-3 for motors and the special contactors ( capacitor contactors)
our TESYS contactors for switching 3-phase capacitor banks for power factor correction are designed for switching single or multiple capacitor banks they conform to standards IEC 60070 and 60831, NFC 54-100, UL, and CSA
About its applications: contactors fitted with a block of early make poles and damping resistors, limiting the value of the current on closing 60 In max, this current limitation increases the life of all the components of the installation in particular that of fuses and capacitors
you will find our TESYS contactors for switching 3-phase capacitors bank PDF from the catalogue to know more about this range
About the range of our Low voltage capacitors (Varplus can ) we have 3 types according to applications and specifications needed ( Varpluscan SDUTY, Varpluscan Hduty, and Varplus can Energy )
you will find in the attached PDF from (the reactive energy management catalog) the part of the selection of the capacitor and the needed contactor for capacitors
About the motor contactors, it's only used for switching ON/OFF the motor conforming to category AC-3 (used for squirrel cage motors ).
Released for: Schneider Electric Saudi Arabia