{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to manually test an output on the Sepam 20 Series

Issue
Need to trip the breaker manually from the front display or software.

Product Line
Sepam 20 Series

Environment
Operating an output

Resolution
This pdf is a step-by-step procedure on how to manually activate an output using only a Sepam 20 relay with the advanced display (UMI) or SFT2841 commissioning software. No current/voltage injection is required in order to perform this task.

Schneider Electric Saudi Arabia

Attachment(s)
MANUALLY_Testing_Outputs.pdf [104.73 KB]