{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the part numbers for the cables that are used in a front face connection with the SEPAM relays?

Issue
A user would like to know the part numbers for the cable that is used to communicate with a SEPAM relay using the front face connection and a computer

Product Line
SEPAM Series 20 ,40, 50, 80

Environment
SEPAM front face communication

Cause
A user would like to order a replacement cable to communicate with the relay

Resolution
For the Old PS2 connection:
The following 3 cables are needed for a front face connection to the SEPAM Relays.
- CCA783 Cable for PC (RS232 connection) to relay connection
- TSXCUSB232 USB/RS232 interface (CCA783 cord must be ordered separately)(USB to serial cable (CCA783) converter)
CCA783


For the new Mini B to USB connection:
-CCA784 Cable for PC to relay connectionCCA784

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: