{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Problem of no immediate recognition of a change of password with SFT 2841.

When a password is modified on the DSM UMI of the Sepam 1000+ during the connection processing of the SFT2841 software to this Sepam, SFT2841 software doesn't take into account the modification and still accept the previous password.
Ask for "disconnection" and then "Connection" again by using SFT2841,such as this one takes into account the new password.

Problem on SFT2841 v4.0 only . Corrected on version 4.1.

Re-published to revised security level: 17 June 2008 by DRM

Applies To: Sepam 1000+ (Sepam Series 20 and Sepam Series 40)

Original Author: FK

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166709 V2.0, Originally authored by FrKr on 06/18/2008, Last Edited by DaMi on 06/18/2008
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software), Sepam series 40, Sepam series 20

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.