{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to open the SFT 2841 with all the connection parameters already defined?

Goals and Symptoms

Is it possible to open the SFT 2841 with all the connection parameters already defined ? In other words, one wants to start the SFT 2841 from under their SCADA and the have the SFT 2841 software automatically connect to a given Sepam unit (without inserting manually the connection parameters like IP address of the gateway and Sepam Modbus address)

Causes and Fixes

It is not possible . You do need to set network configuration in SFT2841, before being able to get distant connection via IP address

Re-published to revised security level: 17 June 2008 by DRM

Applies To: SFT2841

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL177774 V2.0, Originally authored by KBAdPM on 11/05/2007, Last Edited by DaMi on 06/18/2008
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software)

Schneider Electric Saudi Arabia