{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
For Sepam 80: what is the correct order for adding the accessories MSA 141, MET 148, DSM 303, and MCS 025?

Goals and Symptoms

For Sepam 80: what is the correct order for adding the accessories MSA 141, MET 148, DSM 303, and MCS 025?

Causes and Fixes

The Sepam 80 has got 2 Ports. Using these, it is always possible to be able add all the different accessories that one might need for the Sepam 80.
On the D1 port, connect in order the MSA 141, next 1 or 2 MET 148 ( 1 MET 148 if you use also DSM 303) and next at the end the DSM 303

On the D2 port, connect in order the Second MET 148 and the MCS 025 at the end.

Rule:
You can connect a maximum of three accessories on each port (D1 or D2).
The DSM 303 and the MCS 025 have to be always at the end of this chain. So if you use these 2 Accessories DSM and MCS on same Sepam 80, you have to use necessarily the 2 ports ( i.e. set the DSM at the end of D1 and set the MCS 025 at the end of D2)

AEDL3


Legacy KB System (APS) Data: RESL201116 V1.0, Originally authored by DaMi on 01/22/2010, Last Edited by DaMi on 01/22/2010
Related ranges: Sepam accessories, Sepam series 80

Schneider Electric Saudi Arabia