{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the TCSEAK0100 kit used for?

Goals and Symptoms

WHAT IS USE THE KIT TCSEAK 0100 FOR ?

Causes and Fixes

The KIT TCSEAK 0100 is an Adaptation Cable which enables a serial RS 232 connection from PC to the Edgeport EGX 100 or ECI 850 ?
This connection via the TCSEAK0100 cable to RS 232 Port enables the setting or re-setting of the Edgeport EGX 100 or ECI 850 and In particular to access again at the IP Address of the Edgeport in case of losing it, for example. It is good for communications connections for all other types of configuration needs as well.

The documentation for this kit can be found at https://www.se.com/ww/en/download/document/63230319205/.

A scanned version of this document is also attached below.

Schneider Electric Saudi Arabia

Attachment(s)
DOC_TCSEAK0100_EN_SP.pdf [98.21 KB]