{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is circuit breaker control and how is it enabled in SEPAM devices?

Issue
User would like to learn more about circuit breaker control and how it is enabled in the SEPAM relays

Product Line
SEPAM series 20
SEPAM series 40
SEPAM series 80

Environment
SFT2841

Resolution
Circuit breaker control is a function available on the SEPAM series relays to enable the remote opening and closing of circuit breakers. ​When this function is enabled, I11 and I12 (SEPAM 80 I101 and I102) are automatically locked into being the open and closed status contacts from the breaker. If these contacts are not connected when CB control is enabled the relay will return a Trip Circuit Fault.
Figure 1

To enable circuit breaker control, connect to the SEPAM relay using SFT2841 and access the program logic screen. The function is labeled CB Control: here it may be enabled or disabled as needed.

Figure 2

Schneider Electric Saudi Arabia