{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where to download the latest version of SFT2841

Article available in these languages: Czech

Issue
Need the settings software for SEPAM 20, 40, 50, 60, and 80 series.

Product Line
SEPAM SFT2841

Environment
Configuration tool, settings software

Cause
Where to download the latest version of SFT2841

Resolution
Click here to download the latest version of SFT2841 v17.4
Note: for customer with the latest build of Windows 10, or newer OS.
When installing the software use your previous serial number
The install will not complete without a valid serial number.  If this is your fist install of this software you will need to enter 0647740-08 as the serial number.

Schneider Electric Saudi Arabia