{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to build a part number for the SEPAM relays

Issue
Need to create a SEPAM part number.

Product Line
SEPAM 10, 20, 40, 50, 80

Resolution
The Sepam relays are highly modular and hence the part number may be complex. To assist with this download the attachment below called the Sepam Product Selector Tool. One is for the US and the other is for Canada.

Schneider Electric Saudi Arabia

Attachment(s)
2018 SEPAM US Product Selector v1_4_8.xlsm [3.75 MB]
2018 SEPAM CA Product Selector v1_4_8.xlsm [3.75 MB]