Search FAQs
Compatible I/O units for VAMP 221
Issue
User needs to know which I/O units are compatible with VAMP 221
Product Line
VAMP 221
Environment
I/O units
Resolution
The following I/O units are compatible with VAMP 221. Details for each unit are provided below.
- VAM 12L accommodates up 10 arc APS_SENSORS, 3 APS_SENSORS have dedicated trip outputs
- VAM 12LD accommodates up 10 arc APS_SENSORS, 3 APS_SENSORS have dedicated trip outputs
- VAM 10L accommodates up 10 arc APS_SENSORS
- VAM 10LD accommodates up 10 arc APS_SENSORS
- VAM 3L accommodates up to 3 fiber loops
- VAM 3LX accommodates up to 3 fiber loops with sensitivity adjustment
- VAM 4C accommodates up to 3 current transformers
- VAM 4CD accommodates up to 3 current transformers
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: