{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the modules that may be used with the ADVC Controller?

Product Line
ADVC 2

Resolution
FTIM - The FTIM (Fast Trip Input Module) is an ADVC Controller Range accessory that accepts external control signals
from third party devices. It provides optically isolated inputs. These allow connection of an external protection relay
or Remote Terminal Unit (RTU). The electronic circuit is installed in a die cast, sealed enclosure which is attached
to the upper accessory mounting tray of an ADVC ULTRA controller.
It is possible to interface external trip, close or block signals to the recloser controller via the FTIM.

IOEX -The IOEX (Input Output Expander Module) is an ADVC Controller Range accessory that accepts external control
signals from third party devices. It provides optically isolated inputs and voltage-free outputs. These allow
connection of an external protection relay or Remote Terminal Unit (RTU). The electronic circuit is installed in a die
cast, sealed enclosure which is attached to the upper accessory mounting tray of an ADVC ULTRA controller.

Schneider Electric Saudi Arabia