{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the default passwords for the ADVC controllers?

Issue
A user would like to know the default passwords for the ADVC Controllers

Product Line
ADVC Controllers

Environment
Security

Cause
A user would like to know the default passwords for the ADVC Controllers

Resolution
There are four unique passwords that are default on the ADVC controllers:
System = WSOS
Software = CAPM
Front Panel = AAAA
Remote = 000000

Note: These passwords are configurable via the front panel and the WSOS software


Legacy KB System (APS) Data: RESL211667 V1.0, Originally authored by DaFr on 06/04/2013, Last Edited by DaFr on 06/04/2013
Related ranges: Others protection relays

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.