{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What versions of the TSX Micro/Premium firmware needed in order to use the PCMCIA memory backup card TSXMFPB096K?

Issue:
Versions of the TSX Micro/Premium firmware needed in order to use the PCMCIA memory backup card TSXMFPB096K


Product Line:
TSX Micro/Premium, PL7


Resolution:
The TSXMFPB096K can be use on the Premium (TSX57) Version 5.5 and later and for the Micro (TSX-37) Version 5.1 and later.

Schneider Electric Saudi Arabia