{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ProWORX 32 Server limitations

Issue
ProWORX 32 Server limitations

Product Line
ProWORX 32...All versions

Environment
Windows 7

Resolution

The following limitations have been found on the ProWORX 32 server.

  • If the server is being used for communicating to the PLC:
The limit is 3 for connecting to the PLC via the server and 5-8 users for
connecting to the server for puts and gets at the same time that the clients
are connected to the PLC via the server.
  • If the server is used only for project storage and retrieval (the server is not used for
communicating to the PLC):

No limitations on number of users simultaneously connected with
either Modbus Plus or TCP/IP other than what is allowed for the server PC's
Microsoft Windows operating system's TCP/IP connections and the Modbus Plus
Adapter card.
  • Maximum number of users configured on the server:
  • No limitations.
  • Maximum number of projects stored on the server.

No limitations other than the hard drive free space capacity.

Schneider Electric Saudi Arabia