Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Unity Pro: What is the use of the BAK file?

- When you open a .stu file and make modifications, you save the current file.  Two files are actually created:

- a .BAK file which is a copy of the .STU file that you  had opened.
- a new .STU file with the modifications
- If you make several saves during the modifications, the content of the .BAK file is always equal to the n-1 save
- This file can be useful in the event of a crash. You are able to retrieve the previous application easily modifying the .BAK type of this file in .STU type

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: