Search FAQs
Can I use a HART enabled device with the M340 analog input module?
Yes, the BMXAMI0800 and BMXAMI0810 modules will support analog signals with HART protocol.
If HART information is part of the signal to be measured, a Telefast interface
ABE7CPA31E has to be used to filter this information which would disrupt the analog value.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: